Action Deployment
Overview
The final step is Action Deployment. This view displays a time-series trend with the following information:
-
Actual
The original source data for the model target selected during the modeling step. -
Action Output
The projected model target as optimized by the action model constructed during the Knowledge Fusion step. If no Action model exists, Action Output will not be displayed.
NOTE: In order to be able to display Action Output, the action model must contain at least one rule. -
Setpoint
The set setpoint as specified during Benefit Estimation. If Benefit Estimation has not been completed, no setpoint will be displayed. -
Optimized
The optimized process output as determined during Benefit Estimation. If Benefit Estimation has not been completed, this trend will not be displayed.
Export Options
-
Export Blueprint
Export the blueprint as used by the Continuous Troubleshooter project for further editing in the Architect. This blueprint can be further extended to a large scale solution Action Object. -
Export Action Object
Export the Action Object as used by the Continuous Troubleshooter project. -
Export Model
Export a trained model as an XML file to a location which you specify. The model can now be opened in the Architect for further editing.
Related topics: